Other Parts Discussed in Thread: TPS650250
Hi,
we use all 3 DCDC Converters on the TPS65023 as follows:
Supply Voltage = 5V
------------------------------
DCDC1 = Should be 1.2V but is 2.0V
DCDC2 = 1.8V
DCDC3 = 3.3V
We're using Resistor dividers to set the required output. Which is working fine for DCDC2 / 3 but not for DCDC1.
DCDC1 is at 2.0V all the time. We even set DEFDCDC1 to GND which should defaults the output to 1.2V but it stays at 2.0V
There is no other source of 2.0V on the board so it´s unlikely a short-circuit or something.
So the question is.. why is DCDC1 2.0V ?
Edit 1: DCDC1 has 1V Threshold on DEFDCDC1 which should be 0.6 like DCDC2 and 3 ?
Edit 2: We read out the I2C registers and the chip is reporting that all voltages are within regulation which is not the case in reality.
Additionally, register address "0x05" Bit 6 (Core ADJ allowed) is set to "0" but the default is "1" ... we never set any bits there...
Edit 3: Mesurement of Power-On behaviour