Other Parts Discussed in Thread: TIDA-050047, , BQ25790
Aside the differences stated in the datasheet and the package. Are there any other differences between them? In TIDA-050047, there is some words as below:
The BQ25792 is an integrated switched-mode buck-boost battery charge management device intended for 1- to 4-series cell Li-ion and Li-polymer batteries. The charger features a narrow VDC architecture (NVDC) which allows the system to be regulated to a minimum value even if the battery is completely discharged. Additionally, the BQ25792 supports input source detection through D+ and D- which is compatible with USB2.0, USB3.0 power delivery, non-standard adapters, and high voltage adapters. With dual input source selection, USB OTG support, and an integrated 16-bit multi-channel analog-to-digital converter (ADC), the BQ25790 is a complete charging solution.
You see, it says BQ25792 first, but suddenly BQ25790 come out, it make me feeling there may be some differences in their function, if it's not a typo. Is BQ25790 a *complete* charging solution but BQ25792 not?
Thanks.