This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8733: PGOOD is fixed at Low.

Part Number: LP8733
Other Parts Discussed in Thread: TIDA-050038

Hi,

We desighed a circuit consist of LP873347RHDT and TPS6521825RSLT for i.MX8M mini.
But PGOOD is fixed at Low.

BUCK0 and BUCK1 output is correct voltage.
So, I think there is a problem with LDO input or output.

Since LDO0 and LDO1 are not used, the connection is as follows.

VIN_LDO0 +5V(=VANA)
VIN_LDO1 +5V(=VANA)
VOUT_LDO0 NC
VOUT_LDO1 NC

Can you give me an idea of what is wrong with the circuit.

In drawing of TIDA-050038,  VIN_LDO connected to the +3.3V. Is this a problem?