Part Number: LM20136
Other Parts Discussed in Thread: TPS62812-Q1, TPS628512
I am using the formula on page 16 of the LM20136 datasheet to calculate the minimum inductor with the values below. I am getting a minimum inductor value much larger (6.7uH) that what is recommended by the WEBBENCH and design spreadsheet (1uH). Am I missing something? I know my continuous output current (for this instance) is well below the maximum rated output current but seems like the equations should align between the tools.
Vin=5V, Vout=1V, ripple current=0.3A, around 40% of max output current, switching freq= default (410kHz)
Thanks.