Other Parts Discussed in Thread: LM5176
Hi!Ti engineers!
What is the difference between lm5175 and lm5176?At present, the supply of lm5176 is difficult.Can lm5175 be used instead of lm5176?The current design specification is 8 ~ 36V input and 12V / 6A output.The specification lm5176 can meet the design requirements.I use WEBENCH ® Power designer, lm5175 can not meet this demand.Lm5175 can only realize 8 ~ 36V input and 12V / 3A output.Can lm5175 meet the requirements of 8 ~ 36V input and 12V / 6A output?Thank you for your reply.