Hi team,
I think there is mistake in LM61460-Q1 design tool excel file. When I input ESR of Cout = 0 and the bode plot will be the straight line, but I dont think this is the correct result. May you help check the formula?
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
I think there is mistake in LM61460-Q1 design tool excel file. When I input ESR of Cout = 0 and the bode plot will be the straight line, but I dont think this is the correct result. May you help check the formula?
Roy
Hi Roy,
It is not realistic to expect ESR of 0 for Cout since even MLCC with the smallest ESR will have some value usually in 1-3mOhm.
As such it is suggested to use 1mOhm in that cell.
It looks like the Co output electrolytic cell is okay if you put 0.0000001. For all intents and purposes, this is basically almost no electrolytic capacitance. I'd suggest keeping cell 100 as 0.0000001 if you are not using an electrolytic.
The bode plot curves should be okay for a majority of common use case applications.
Regards,
Jimmy