This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24073: Inquiries about replacement products (delivery available)

Part Number: BQ24073
Other Parts Discussed in Thread: BQ24232HA, BQ24074

Hi, TI Support Team

A customer company is looking for a replacement product due to a delivery issue during development with the BQ24073RGTR product.

Please recommend a product that can be pin-to-pin as much as possible.

Please check the product with a relatively short delivery time.

Thanks.

Regards,

MJ

  • Hi  MJ,

    There is the BQ24232HA device that is the is the same for the most part aside from the ITERM pin in place of the TD pin and has a charge range of up to 500mA.

    Any of the BQ2407x devices will be pin to pin as well (not the T devices that are utilize as a voltage based TS method). You just need to consider the pin differences as there are small differences. The closest one would be the BQ24074 but it has the ITERM pin which allows for the programming of the termination current threshold.

    Any of these devices can be ordered from the ti e-store

    Best Regards,

    Anthony Pham