Other Parts Discussed in Thread: LM5022
Hi all,
I want to use LM5020 to control flyback converter. I have some question for this IC. Please help me.Thanks!
Input voltage is DC 30V to 100V. Output is 12V/100W.
1.When I turned on, Vin supplied power to the LM5020. When Vcc is established, the Vin power supply is cut off internally, and Vcc supplies power to the LM5020. Is this right?
2.(Premise Vin stays on all the time), continue question 1. When I disconnect Vcc, will the internal power supply to LM5020 by Vin be changed? Will the LM5020 work normally at this time? Or do I need to reconnect Vin for the LM5020 to work normally?
3.I want to set up a protection circuit. In addition to grounding UVLO, which IC Pin can achieve this effect?
4.Will LM5020 always detect the presence of Vin, or is it only useful before Vcc is established?
5.If my protection is automatically restored, I only need to pull the UVLO to the ground, wait for the recovery time, and then pull the UVLO high, will the LM5020 operate normally? There is no need to reconnect Vin.
Sorry, it is the first time to use this IC, any comments are welcome, thank you
Micky