This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51275: Two output voltage regulation

Part Number: TPS51275
Other Parts Discussed in Thread: TPS51395P, TPS51395, TPS566231, TPS566238

I see TPS51275 has two output control, and I want use it to output 5-V/3-A in both two channels.

My question is : 

(1) Why the datasheet shows the output voltage is 5 V in channel 1, and is  3.3 V in channel 2? Can't I regulate the two output voltage by feedback resistor divider? 

(2) Will two 5-V/3-A output affect two LDO outputs in VREG5 (5-V) and VREG (3.3-V)?

Thanks very much for your time and supporting!