This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC217xx and ISO5x5x are both Single-channel isolated gate drivers with advanced protection features.
What are the differences in performance and feature set between the two families, as well as between the familial variants?
Part numbers covered:
UCC21710, UCC21710-Q1, UCC21750, UCC21750-Q1 & UCC21759
UCC21732, UCC21732-Q1, UCC21736-Q1, UCC21739-Q1
ISO5452, ISO5452-Q1, ISO5852S, ISO5852S-Q1 & ISO5852S-EP
ISO5451, ISO5451-Q1, ISO5851 & ISO5851-Q1
Please download our portable comparison guide for our Single-channel SMART driver families!
Differences between UCC217xx and ISO5x5x-v14.pdf
The document is copied below