This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56C215: TPS56C215

Part Number: TPS56C215

1V_design.docx

We have a conducted emission noise on our power cable due to 1V regulator – 1.2MHz.

We want to check the other modes to see the influence: 400KHz & 800KHz. (see DS page 16).

Is it acceptable as EyeQ4 1V (U7 page#2) requirements are very strict ?

Please see attached.

Thanks,1307.tps56c215.pdfEyeQ4 SoC Digital Core Power Rail.pdf

Haim G.

  • Hi Haim,

    This device is not designed for low noise application. So we didn't have detailed evaluation for it now. But first I want to understand which is the (U7 page#2) requirements for EyeQ4 1V. I didn't find the word "U7" in the attached files.

    Thanks,

    Andrew

  • Hi Andrew,

    Thank you.

    U7 is the ref. des. of TPS56C215.

    Please see attached.ME8_PS_only.pdf

  • Hi Andrew,

    What is the difference between FCCM and DCM modes ?

    Thanks,

    Haim G.

  • Hi Haim,

    When there's large load current (load current larger than half of the peak to peak value of inductor ripple current) for the device, there's no difference for DCM and FCCM mode. The difference is only when there's light load for device. 

    DCM mode doesn't allow the negative inductor current, so when the load current is smaller than half of the peak to peak value of inductor ripple current, the device will enter discontinuous mode. Switching frequency will become lower with light load and that can help to increase the efficiency at light load. But the output voltage ripple will also increase at light load. 

    FCCM mode allows the negative inductor current, so it could keep same switching frequency from light load to heavy load. The output voltage is almost same with changing load, but the efficiency at light load will be worse than DCM mode.

    About the requirement for TPS56C215 that you mentioned, if my understanding is correct, is that referred to the Table4 or Table 5 in the EyeQ4 SOC digital core power rail documents?

    And which one is the requirements for the U7 power rail? Table 4 or Table 5? Is there any other requirements not mentioned in this table?

    Thanks,

    Andrew

  • Hi Andrew,

    Thanks for the detailed answer.

    Please refer to table 4.

    Haim G.

  • Hi Andrew,

    Another question:

    What is the max. ripple for DCM and FCCM for the table 4 EyeQ4H requirements ?

    Thanks,

    Haim G.

  • Hi Haim,

    If you want to get the transient peak to peak value for TPS56C215 under table 4 requirements, I am afraid we don't have the data on hand. The most effective way is to use Webench to simulation the load transient performance.

    Thanks,

    Lishuang