This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2750: LM2750-ADJ Boost

Part Number: LM2750
Other Parts Discussed in Thread: TPS60130

Dear *,

can we generate 3.6V from 3.3V with LM2750-ADJ? Or do you recommend a different Charge pump inductor less IC?

Best Regards,

David. 

  • Hello David,

    You can create 3.6V from 3.3V with a charge pump, but the efficiency will be in the range of 54% as the charge pump is doubling the input voltage and then dissipating the not needed energy. This is valid for every charge pump doubler. You might have a look at the TPS60130 for a better efficiency at these voltage levels.

    Best regards,
    Brigitte