Hi,
1. What is the recommended for choosing the UV/OV Threshold?
2. Suppose I have a 2 power supplies with 1.0V and 3.3V, is the UV/OV Threshold need to be according the present % like 5% UV and 5% OV or like 150mV_UV and 150mV_OV or like the load recommended voltage or like the load absolute maximum voltage for both power supplies?
It can be a problem if I set the sequencer for shutdown without to choosing the right UV/OV parameters.
Please help me to understand if there is a rules about it.