Hi Experts.
I have designed a buck converter with the below specifications.
Vin: 18V to 36V (Vin Nominal is 24V)
Vo: 12V at 5A.
I am using the same circuit as recommended by Webench. The only difference is, I have connected the PGOOD to MCU's input pin which is pulled to 3.3V. Whenever I am driving the current, the voltage is dropping to ~4 to 6V.
What Can go wrong here?
Regards
Vishal