Hi Team,
May I know the Efficiency Value/Range for TPS51200A-Q1, for the following condition
Input Voltage : VLDOIN = 1.5V ; VIN = 3.3V ; REFIN = 0.75V
Output Voltage : VO = 0.75V ; REFOUT = 0.75V
Output Sink/source Current = 0.3 to 0.6A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
May I know the Efficiency Value/Range for TPS51200A-Q1, for the following condition
Input Voltage : VLDOIN = 1.5V ; VIN = 3.3V ; REFIN = 0.75V
Output Voltage : VO = 0.75V ; REFOUT = 0.75V
Output Sink/source Current = 0.3 to 0.6A
Hi Jayakrishnak,
TPS51200A-Q1 is an LDO, the efficiency from power stage is just Vout/VIN.
If you want to take into account of the bias current from 3.3V input (~0.7mA), then it will be (Vout*Iout)/(Vin*Iout+3.3V*0.7mA)
For 0.6A output current, the efficiency is about 49.87%
For 0.3A output current, the efficiency is about 49.74%
Regards,
Weidong