What is the ICCQ of the fuel gauge if the CE is de-asserted and the FG is in shut down?
Section 7.5 doesn't specify the CE pin status.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the ICCQ of the fuel gauge if the CE is de-asserted and the FG is in shut down?
Section 7.5 doesn't specify the CE pin status.
NIcholas,
When the CE pin is low the gauge is 100% off. There should be no ICCQ outside of some leakage which would be minimal and vary part to part.
Thanks,
Eric Vos