Hello Experts,
Customer has question as follows. Would you please answer them?
1. What are the conditions for completing the efficiency curve on the spec sheet? EVM may vary, but it's around 63%@10mA.
2. Why do you recommend metal alloy inductors?
3. Is there a way to get better efficiency at low current (10 mA)? (Vin=3.3V, Vout=-5.0V, Imax=120mA)
4. Customer measured the quiescent current of EVM, the result was 9mA(Vin=3.3V). Then he changed the inductor to NRS3015T4R7(TAIYO YUDEN) and measured the quiescent current again. The result was 14mA. Also, he measured the quiescent current by changing the inductor to NRS4018T4R7, the result was 12mA. So it seems that the inductor affect the quiescent current at low load current. Do you think that the core material difference is one of the reason? Or does it have another factors?
Best Regards,
Fujiwara