This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryo
Yes the difference is the current rating between the devices, maximum adjustable frequency (500kHz vs 2.2MHz), and the default frequency when RT is floating (400kHz vs 500kHz)
Functionality, features and the pinouts between the devices are the same.
I hope that helps
Thanks
-Arief