This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, we decided to use the TPS61178RNWR since it had a high output current, relatively high startup voltage of 2.7V (so doesn't draw massive current when Vin < 1V). We purchased a EVM kit and did some tests which showed it should have no problem with driving 4A output. Chip only warmed up to 30C or so after half an hour.
We designed using the Altium design files which saved heaps of time. Anyway, when the board arrived, hard to find stock of this chip so we purchase some from Utmel in China. Code on chip shows 15RI. The first 3 boards we had issues with - the output was supposed to be 14.0V (R1 = 1M // 5M1 otherwise same parts as EVM) . The first 3 boards gave outputs of 20V, 13.6V and 12V. Measuring the feedback resistor, we could see the first board had a Vref of 1.78V instead of 1.198V. Is there any reason for this - we are thinking maybe the chip was too hot during assembly or else chips are counterfeit. Any help would be much appreciated. Thanks
Hi Fergus,
it seem the circuit is not well soldered. please double check if the IC pin is well connected to the board.
The chip looks very well soldered to me - can you point out where the bad solder joint is? Also, I am not sure how a bad soldering connection would make the Vref rise to 1.8V.
Hi Fergus,
I can't find problem in the solder. but such inconsistence behavior is normal caused by solder or IC damaged.
it seem the layout is not good. did you follow the suggestion in the datasheet and the EVM to do the PCB layout. layout is very critical to the normal operation of a switching converter.