This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
I want to check about Reverse current Block function for the TPS25221.
If the VIN is 0V when the device is disabled, is the device add any stress?
I’d like to confirm about VIN<ONT is okay, even if VIN=0V.
Regards,
Sato
Hi Sato,
That's fine as it's back to back FET structure inside.
It can withstand the reverse voltage below ABS.
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.
Thanks.