This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck Converter for IBB Configuration with high efficiency and low ripple at light load

Other Parts Discussed in Thread: LM63615-Q1, LMR36503-Q1

I posted I need help replacing a Maxim power part for an automotive customer's radar system.  I am planning to use a standard buck in IBB configuration as discussed in:

Create an Inverting Power Supply From a Step-Down

Using a buck converter in an IBB topology

Their current design uses the MAX16945TGUT/V+.  This chip is an inverting charge pump that will invert 5.4V to -5.4V. Here is the datasheet for the Maxim part: Datasheet.  My goal is to pitch one of our parts to replace the Maxim part.  The efficiency of the MAXIM part is around 90% at nominal load 5V @10mA.  Ripple is also a very important consideration for this system.

 

I have been looking at a few buck converters: TPS54061-Q1LM5165-Q1 and LMR36503-Q1.  The LMR36503-Q1 is the only one that is in stock.  Unfortunately, they are all out of stock.  Since this is for automotive, I have ruled out the buck converters with higher Iout(max) because the frequency will drop into the AM band for the Iout(nom) = 10mA of my system.  Is that correct? 

Do we have any automotive grade bucks that can:

  • Operate in IBB configuration
  • Forced Frequency to stay out of AM band 
  • Low current efficiency >= 90%

By the way, we have a few automotive charge pumps, but they don't meet the input voltage requirement of 5.4V.  

I'd appreciate any help.