I need to monitor 0.6V power rail. Is there a voltage monitor, supervisor, reset IC that can do this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need to monitor 0.6V power rail. Is there a voltage monitor, supervisor, reset IC that can do this?
Yes, there are several voltage supervisors we have in our portfolio that can monitor 0.6V and lower. Please see below:
TPS3700 - High voltage (18V) window voltage detector with internal reference for over and undervoltage monitoring (Adjustable threshold voltage requiring external resistors that can monitor down to 400mV)
TPS3701 - High voltage (36V) window voltage detector with internal reference for over and undervoltage monitoring (Adjustable threshold voltage requiring external resistors that can monitor down to 400mV)
TPS3703 - High Accuracy Overvoltage and Undervoltage Reset IC With Time Delay and Manual Reset (Sense down to 500mV)
TPS3710 / TPS3710-Q1 - Wide VIN Voltage Detector (Adjustable threshold voltage requiring external resistors that can monitor down to 400mV)
TPS3711 - 36-V Voltage Detector (Adjustable threshold voltage requiring external resistors that can monitor down to 400mV)
TPS3808 / TPS3808-Q1 - Low-Quiescent-Current, Programmable-Delay Supervisory Circuit (Adjustable threshold voltage requiring external resistors that can monitor down to 405mV)
TPS3899 / TPS3899-Q1 - Nano-Power, Precision Voltage Supervisor, Push-Button Monitor with Programmable Sense and Reset Delay (Adjustable threshold voltage requiring external resistors that can monitor down to 505mV)
TLV841 - Small Size Nano-Power Voltage Supervisor in WCSP Package (SENSE variant - Adjustable threshold voltage requiring external resistors that can monitor down to 505mV)