This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27201: Max current required for UCC27201 in the worst case

Part Number: UCC27201
Other Parts Discussed in Thread: LM34927,

Hi Team,

I'm looking into the possible max current required for UCC27201 (VDD) to see if designing power supply with LM34927 (600mA DCDC) is okay.

It looks the IC itself consumes approximately 1.6mA (0.8mA+0.8mA) under f 500kHz and no load on PWM outputs. And this device is max 3A source capability with load. Does this mean UCC27201 VDD pin requires the current of 1.6mA + 3A in the worst case? If so, it looks I cannot use LM34927 to supply VDD of UCC27201. Could you advise?