Other Parts Discussed in Thread: TLV702,
Hello team,
I received a inquiry from my customer about the spec difference between TLV702 and TLV702-Q1.
Are their any spec difference between these catalog and Q1 products?
In the data sheet, the shutdown current was different as the following values:
TLV70225QDSERQ1:2.5uA(max)
TLV70225DSER:2uA(max)
I assumed that this is a difference due to the test conditions where Q-1 was tested at 125°C and catalog was at 85°C. If Q-1 is also at 85°C, it will be the same specification as catalog. Please let me know if my assume was wrong.
If there are any differences other than that of the AEC-Q100 test conditions, please let me know.
Best Regards,
Ryotaro Fukui