Since TPSM84424 is a QFN Open Frame, Can components be places below the TPSM84424 module?
If yes what is the maximum height possible for such scenario?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Since TPSM84424 is a QFN Open Frame, Can components be places below the TPSM84424 module?
If yes what is the maximum height possible for such scenario?
Hello,
Components cannot be placed below the TPSM84424 module on the same layer of the board. On the opposite layer, components may be placed underneath the module. The substrate of the TPSM84424 has metal pads underneath that are soldered to the board and do not allow for component placement under the device on the same layer.
Regards,
Alec Biesterfeld