Hello,
I am using "TPS65265RHBR" Buck Switching Regulator with 3 channels.
The first channel (LX1) was given to 1.8V. (max current requirement is 600mA.)
The second channel (LX2) is given to 1.5V. (max current required is 100mA.)
Third Channel (LX3) given to 1.1V. (Max current required is 100mA.)
But when i connect to load device 1.8V (LX1) is raising to 2V.
it should be 1.8V actually but it raising to 2V.
Can someone be given suggestions on how to solve this issue?
Regards
NIKHIL