This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54527: Soft start

Genius 4850 points
Part Number: TPS54527


Customer would like to know about soft start of this part.

Please check attached file. We would like to know  value with valration or equation of ? in attached file.

Regards,

Kurasoftstart.pptx

  • Hello Kura,

    The soft start function is adjustable. When the EN pin becomes high, 6-µA current begins charging the capacitor which is connected from the SS pin to GND. Smooth control of the output voltage is maintained during start up. The equation for the slow start time is shown below. VFB voltage is 0.765 V and SS pin source current is 6-µA, these are typical values.

    Where tss is the desired start-up time for your application. 

    For a soft-start an external capacitor must be connected to GND as shown below:

    The value of the capacitor C6 will depend on the desired delay-time you would like to give to your device depending on the application.

    Hope this helps.

    Best,

    Jose

  • 1805.softstart.pptx

    Jose-san

    I attached my understanding of soft start sequence.

    Is my understanding correct ?

    Could you please illustrate tss term to attached file.

     

  • Hello Kura,

    Your understanding is correct. The soft-start sequence defines the time it takes the output to achieve its final target.

    Please illustrate with the below snapshot.

    The green circle shows the time it takes the output to go from low (let's say it's zero) to high (its final target value).

    Hope this helps.

    Best,

    Jose

  • Jose-san

    Thank you for your reply.

    softstart2.pptx

    Please let us know more detail about term of Red circle.

    1.EN to UVLO Clear

    2.UVLO Clear to SS starting point.

    Customer think these term has a equation or some value.

    Regards,

    kura 

  • Hello Kura,

    I read some number out from circuit design.

    This delay time depends on SS cap. Simple equation could be used.

    T= C*V/I

    C = SS Cap,

    V ~= 0.7V, it goes to turn on 1 npn from base to change charging current.

    I ~= 18uA.

     

    For example,

    C = SS Cap = 8.2nF.

    T = C *V/I = 6.8n * 0.7 / 18uA ~= 0.319 ms.

     

    Let me know if it could answer customer’s question. Thanks.

    Best,

    Jose