This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV431A: Differences between TLV431A and TLV431B

Part Number: TLV431A
Other Parts Discussed in Thread: TLV431B

HI Guys

Have a question regards the differences between TLV431A and TLV431B

Customer is using TLV431AIDBZR but due to supply challenges they used TLV431BIDBZR instead but they didn’t work.

Main difference identified is the reference tolerance (0.5% not 1%), but it turns out that TLV431BIDBZR also has a slightly larger maximum IK(min) value.

Would this be a factor or what other differences could be pointed out?

Thanks

Rodney