Hello,
My customer wants to use the LMZ14202H under the following conditions.
- VIN = 28V, VOUT=26.5V , IOUT=1.5A
1. When they run WEBENCH® Designer under the above conditions, an error occurs.
What is the required input/output voltage difference for stable operation of the LMZ14202H?
2. When they tested the above conditions on the custom board, the LMZ14202H works fine.
In this case, can the customer ignore the WEBBENCH error and use the above condition?
Regards,
JH