Dear Specialists,
My customer has a question about LM317 application circuit.
I would be grateful if you could advise.
---
For the 3-terminal regulator LM317DCY, there is a description of 3.5mAtyp and 10mAMAX in the column of minimum output current.
What will happen if it falls below 0.01A?
Oscillation, Regulation or etc.
The application circuit is listed below.
I'm thinking of attaching R1(180Ω) between OUT and ADJ and using it with 1.25V / 180Ω ≒ 7mA output.
Is there any problem?
---
I appreciate your great help in advance.
Best regards,
Shinichi