Dear sir,
Below is our requirement which we have simulated in webench.
So we have simulated for 3.3V/40A.We need to find efficiency at different load or amps like 30A,20A,10A,4A with same circuit which is been designed for 40A.
So we generate schematic for 40A and change load in simulation.
We will get efficiency result printed only for 40A and we don't get efficiency data or graph printed for changed load condition.
Is it possible to get efficiency graph for different load with same circuit?
If we add waveform after simulation also,we will get below waveform data like,
Vsw2,Vcomp1,Vin,Vsw1,Vout1,Iout1,Icout ,Iinductor1,Iinductor2 and Iload.
From above data can we calculate efficiency accurately?
It will be helpful if we can generate efficiency graph for different changed load condition.
Hope you understand the details provided regarding problem we are facing.
Kindly check and provide us best possible solution.
Thank you
Girish K