Hi Support Team,
My customer has the question as follows:
I am confirming the action in case of IC and peripheral component failure.
Could you tell me the action in the following status.
Input voltage is 46V, output voltage is 24V, FB resistor(which set the output voltage level)the above one is 18.7kΩ and the below one is 1kΩ
①When the above one of FB resistor is open, what is the output voltage?(how many volts?)
When the above one of FB resistor is short, what is the output voltage?(how many volts?)
②When the below one of FB resistor is open, what is the output voltage?(how many volts?)
When the below one of FB resistor is short, what is the output voltage?(how many volts?)
③When FB pin is open, what is the output voltage?(how many volts?)
④When it is short between FB pin and GND, what is the output voltage?(how many volts?)
Thanks so much.
Best regards,
Yuki