This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM43601: Webench design not working as expected sometimes.

Part Number: LM43601

Hello TI,

I've been working with a negative DC-DC Synchronous Step-Down Voltage Converter with the LM43601:

Layout design followed from recommendation:

3D view.

I'm using AC/DC power supply of 15V from "IRM-30-15" from Meanwell:

The setup rise time is the following:

At full load: 1500ms.

Is there a problem in the setup configuration of the schematic causing sometimes the voltage stays in +1V output instead of -15V?

I'm guessing the soft-start time can be modified so it can start after the 1.5secs but I'm not sure about it.

Also if I make a short between output and GND in a matter of ms (with a tweezers), it reconfigures the output to -15v working well.

Let me know what can we achieve to always make a reliable output of -15V, it's for an audio application for Opamps.

Best regards,

Héctor.