Other Parts Discussed in Thread: TPS23734
In our design, we use TPS23756 and Flyback topology to accomplish DC12V to DC5V.
We observed that if we remove the DC12 and then reconnect the DC12 immediately, the +5V overshoot up to 5.7V
We think that is because the C383 is not fully discharge, and the soft start circuit is malfunciton.
Is there any way to prevent the overshoot in this scenario?
▲ +5V overshoot while DC12 reconnect immediately
Regards,
CF