Other Parts Discussed in Thread: AMC1100
Hi All,
We want to use the LM5176 Buck-Boost Controller in High voltage application.
VIN=270V-360V
VOUT=340V
IOUT=6A
We are aware that the controller is for 60V maximum, so we plan to do some modifications (such as using high voltage drivers, etc..) so it will be suitable for our requirements.
But we haven't found a solution for connecting the current sense resistor to ISNS(–),ISNS(+) pins due to the high voltage at input/output.
Are there any suggestions for solving the issue?
Thanks.