Other Parts Discussed in Thread: LMR36506
Hi team,
Now my customer is going to use LM36506-Q1 with 50-60V input.
In the case of this level of input voltage, the switching frequency is reduced to around 1.3MHz by frequency foldback function.
In this case, should the customer select the inductor for 1.3MHz switching? It means the inductor should be 22uH rather than 6.8uH which is suggested for 2.2MHz.
Or, 6.8uH or 10uH is okay?
Regards,