Hi support team,
I wanna confirm Ta (MAX).
It is different between "ROC" and "PACKAGING INFORMATION".
Which one is correct?
Page-5, SNAS714C
Page-49-50, SNAS714C
・・・
Regards,
Dice-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi support team,
I wanna confirm Ta (MAX).
It is different between "ROC" and "PACKAGING INFORMATION".
Which one is correct?
Page-5, SNAS714C
Page-49-50, SNAS714C
・・・
Regards,
Dice-K
Hi Dice-K,
I've reached out to the internal team and product engineer to get more insight on this.
From initially inspection I'd suspect that the "Op Temp" is referring to junction temperature since the device can not be operated at ambient temperature of 150C without hitting thermal shutdown with the part switching. As such I think this is a typo or needs clarification, but I'll get some confirmation on this and get back to you when I get more details.
Regards,
Jimmy
Hi Jimmy,
Thank you for your support.
Looking at other data sheets, "Op Temp" in "PACKAGING INFORMATION" seems to be ambient temperature (Ta).
Example. Pages 3 and 17.
www.ti.com/.../tps54225.pdf
Is "PACKAGING INFORMATION" of LMS3655-Q1 a typo?
Best regards,
Dice-K
Hi Dice-K,
That could be the case since those numbers are automatically generated.
Again I'd like to be clear that if the device is in 150 ambient temperature and switching, knowing that the device is not 100% efficient, there will be some power dissipation and as a result the device will increase in temperature.
The datasheet shows a minimum thermal shutdown of 160C so it wouldn't make much sense to operate the device at 150C ambient in any case. As such, I would suggest customers look at the electrical characteristics table for guidance since those parameter/specs have been thorough inspected and the packing information might be a typo.
Regards,
Jimmy