Other Parts Discussed in Thread: BQ24072T
Hi,
I'm including the BQ51013B and BQ24072T to charge single LI-ION battery. RX coil is TDK WR303050-15F5-G (Ls = 12uH, Rdc =390mohm)
When using connect BQ24072T directly from a DC source for battery charging ( charing current 300mA), BQ24072T works well with normal input/outpu current waveform.
When using BQ51013B, the output current of BQ51013B has glitches.
Vrect is aournd 5.7V. Battery charge current sees no problem.
I've looked in to the SCH checklist and other 3 related docs but still can't fix it.
All the parametes on the PCB are same as described in BQ51013B datasheet.
Thanks,
Follin