Other Parts Discussed in Thread: TLC6983, LP5890, LP5860
Hi,
Are MSP430 microcontrollers suitable for use with TLC59581?
We are developing an 16x6 LED matrix for our application
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Akash,
could you please provide more information about your application?
We have two new devices (TLC6983, LP5890), it is all-in-one structure which can achieve multiplexing with external switches. One device can drive 16*16 RGB LED matrix and both can be controlled by MSP430. if the information is not public, you can send it to my email(monet-xu@ti.com).
BR
Monet Xu
Hi Monet,
The application is to glow all LEDs in Blue except one which would be glowing Red
Hi Akash,
LP5860 is the more suitable for you application which supports common anode LED and multiplexing function. And one device can drive up to 11*18 LEDs and don't need external switches.
BR
Monet Xu