This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118EVAL: LM25118EVAL: Radiated noise of LM25118EVAL

Part Number: LM25118EVAL

user6144845
LM25118EVAL: Radiated noise of LM25118EVAL

This is a related question.

Hello.

Although the noise due to the snubber could be reduced, the output voltage fluctuates when the input voltage is set to 30V or higher.
There is a voltage drop of VCC.
As I announced in the previous question, a snubber circuit (10Ω + 2000p) is inserted between GATE and SGND of Q1-Q2 of FET.
Please comment on the insertion location and constants.