I am using the LM5166 (adjustable version) to generate a 6.5V output. Would it be possible to use either 3.3V or 5V fixed versions to generate the 6.5V output? Basically, can I simply recalculate the feedback resistors as if the FB node is 3.3V or 5V instead of 1.223V? Or is there something "special" about the fixed versions that require them to be tied directly to Vout, or can only generate their fixed voltage, or anything else that would ruin the ability to use these as a 6.5V regulator?