This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62802: If using 1uH inductor, will it cause the IC work abnormally?

Part Number: TPS62802

Hi Team,

The input voltage is 3.5V-4.4V, the output voltage is 1.8V. The output cap is 20uF. If using 1uH inductor, will it cause the IC work abnormally?

Best Regards,

Gust

  • Hi Gust,

    For TPS62802, the effective inductance recommended is 0.33uH to 0.82uH. There is a chance for instability when operating outside this spec.

    Best regards,

    Varun