This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3851: TPS3851G50EDRBR

Part Number: TPS3851

In TPS3851G50EDRBR (5 V -operating IC) is it possible to operate as below,

VDD (Pin 1) - Connected with 5V supply.

WDO and RESET(Pin 7 and 8 tied together) - Connected through a pull up to 1.8V supply.

Is it possible to use different voltage for Vdd and WDO (Vpu -Pullup voltage).