Hello Experts,
Can you help to understand what happens to TPS65000-Q1 DC/DC output when VINDCDC rises up (system starts) and falls down (system shuts down) in <0V - >=2.3V> range?
Datasheet gives:
UVLO at 1.72V ~ 1.82V
VINDCDC as 2.3V min.
So it is not clear how IC DC/DC behaves in the <UVLO - >=2.3V> range.
If it helps please account for DC/DC Vout set to 1.8V.
This is needed for syste FuSa evaulation.
Piotr