Hi,
The questions is related to the ISO 16750 standard where there is a momentary drop to 4.5V. How would the output react to the voltage drop?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The questions is related to the ISO 16750 standard where there is a momentary drop to 4.5V. How would the output react to the voltage drop?
Thank you
Hello,
Device would continue to operate down to vin uvlo at 100% duty cycle assuming vout setpoint is higher than vin voltage. When vin falls below vin uvlo, which I assume is somewhere around 6V based on minimum input voltage specification of 6V, then device stops switching and output stops trying to regulate to output set point.