This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Youhao, I come back with some new results.
In a first time, I have tested values you have given for compensation network. I have tried with and without Q36. Q36 doesn't affect stability but is required to obtain a clean 5V power supply.
Without load, I think it runs better, but with a load (47 kR / 406 V = 8.5 mA), system shows oscillations and inrush current can be greater than 3A !
Best regards,
JB
Thanks a lot.
I'm trying to find another transformer. The first one I have installed in this circuit was a Wuerth Elektronik (760895631). Q23 and Q24 were destroyed as inductance of this first transformer was too high (500 µH if I remember). The second one is a hand made transformer (with a TDK toric core) and I think that saturation current is less than expected.
Best regards,
JB
Hi JB,
Thank you for the info. If you have new test results this the TDK transformer, please kindly share.
Best Regards,
Youhao
Hi Youhao,
I think I will add a shunt to measure inrush current in transformer as soon as possible.
Best regards,
JB