Other Parts Discussed in Thread: GPCCHEM, BQ25898
Hi,
I've run the relax / discharge / relax cycle on my battery, submitted the data and gotten a response from TI. However, when I ran the tests I did not do so consecutively. I did the relax cycle first, did some other work, and then I left the discharge/relax cycle to be finished overnight at the office as I went home. I then took the discharge/relax log file and just copy pasted the lines to the end of the first file. The data processing seems to have gone fine, however, the error is 7 %. I was wondering whether that really is due to my battery needing to be profiled by TI or if it is because I didn't do the tests back-to-back?
Note that the 'sample' goes up to 213 and then starts from 1 again as I started the second test. Does this matter?