I am using the TPSM82822SILR in a new design. I use it to generate 1.9V, 3.3V and 4V. For the 4V supply I tried increasing the 100pF capacitor to 1.1nF. but it makes no difference
For all 3 supplies they are disabled when the input is below 2.4V as expected. Above 2.4V the supplies switch on, but the output voltage matches the input voltage so they are stuck in the 100% mode. The voltage on the FB pin does not regulate to 0.6V but follows the output in proportion to the divider. It goes well above 0.6V.
For example, the 1.9V regulator has just under 2.5V on the output when the input is 2.5V. All three designs are similar with only the divider ratio different.
The package marking is GA so ibelieve the correct part is installed.
I would appreciate any help or suggestions as to why the part will not regulate but is stuck in 100% mode.