Part Number: TL720M05-Q1
Other Parts Discussed in Thread: LM5161,
Hi,
We are developing a new automotive product within a temperature sampling circuit, we use LM5161 to step down the auto battery voltage(12V) to 8V, and the secondary power circuit we use a TL720M05-Q1 to regulate 8V to 5V as the power supply for the amplifier IC. But we found the output voltage ripple is very bad. The Vpp value of the ripple is about 100mV, and it can't meet the requirement. The schematic of the power supply circuits and the input voltage ripple photo are shown below. I have measured the ripple of the input voltage, and it is also about 100mV. My question is, why can't the LDO suppress the ripple? The high ESR Cin and Cout capacitors are recommended in the datasheet, I don’t understand the principle very well. Could this be the cause of the large output ripple? Thanks!