Other Parts Discussed in Thread: LM36923H
Hi Team,
Is there a PSPICE model available for the LM36922H?
Thanks!
Connor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
10.1 -10.7 is Chinese notional holiday, our expert will reply you after 10.8. if it's an urgent case, please directly communicate with the person who is assigned.
HI Frank,
Understand. Thank you for the update. Please see an additional question below:
Also I would like to know if I should pull the PWM pin to ground or leave open, if we are not using this input.
I did not find anything in the datasheet about configuring this pin when only using I2C to control the driver.
Thanks!
Connor
Hi Frank,
Following up on the above. Is there a SPICE model for the LM36922H?
Also, an additional question can be seen below. Let me know if you need more info.
I am going to design with the LM36922H as the primary part, and use the LM36923H as the alternate since it is pin functional compatible. In this application I don’t need the 3rd string of the LM36923H.
I have more questions:
Thanks!
Connor
Hi Connor,
Sorry for late reply. There have some miscommunication on work hand-over.
For PSPICE model, LM3692x do not have one.
If PWM input is not used, Brightness mode bits need to be set to 00 (brightness register only) and PWM pin can be floating or to GND.
If the third pin is not used, LED3 enable bit need to be disabled and both floating and connecting to GND are OK.